Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Was the NetShelter SX AR33xx roof redesigned in 2010?
Issue:
Newer NetShelter SX AR33xx cabinets have a different roof than older models.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
In 2010 the roof of the NetShelter SX AR33xx cabinets were redesigned to allow more room for cable access.

Resolution:
See attached file

Schneider Electric Nigeria

Attachment(s)
20131206 NetShelter AR33xx Roof Redesign.pdf [560.51 KB]