How can we help you today?

The fan operation for the Back UPS XS/ NS / RS ""G"" / ""GI" models.

Issue:

What is the fan operation of the Back UPS XS/ NS / RS ""G"" / ""GI"" models?

Product Line:

Back-UPS Models BX / BN and BR

Environment:

Effective manufacturing week 42 of 2010, For the BX/BN/BR ""G"" / ""GI"" models of Back UPS, the fan will operate only during AVR Boost operation.

Cause / Resolution:
AVR Boost (88~105vac) Percentage Loading Fan Duty Cycle
0% 50%
40% 62.5%
60% 75%
100% Always On