Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a way to get more torque out of the motor when running at lower speeds with an ATV312 drive?
Issue:
How to increase the torque out of a motor when running at lower speeds with an ATV312 drive

Product Line:
ATV312

Environment:
All

Cause:
More torque

Resolution:
First, verify that the motor data is correct in the drC menu.  Then set UFt to L.  In the SEt menu, increase UFr to provide higher torque output.


Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings