Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the dissipated power heat loss for the ATV61 drives?
Issue:
ATV61 dissipated power heat loss

Product Line:
Altivar ATV61

Environment:
All open type ATV61 drives

Cause:
Needs to know what the dissipated heat loss is for the Altivar ATV61 drives for sizing an AC unit.

Resolution:
See the attachment for dissipated power with drive mounted inside of the enclosure and dissipated power with drive mounted in flush mounting optional mounting kit.

Schneider Electric Nigeria

Attachment(s)
Power Loss ATV61.pdf [57 KB]