{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the adjustment ranges for the dials on an ATS01N1..FT?
What are the adjustment ranges for the dials on an ATS01N1..FT?

Issue :
Adjustment ranges for Schneider-Electric recommend for Altistart Soft Starters?

Product Line :
Altistart Soft Starters

Environment :
Open style Soft Starters

Cause :
Adjustment Range

Resolution :
For the START TIME dial, setpoint A is 1second and setpoint E is 5seconds.  There is a linear relationship from A to E setpoints.
For the INITIAL VOLTAGE dial, setpoint A is 30% and setpoint E is 80% of full voltage.  There is a linear relationship from A to E setpoints.

Schneider Electric Nigeria