Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the default control board for the ATV212 (or ATV21) drive be purchased as an individual part?

Article available in these languages: Spanish

Issue:
Control board for the ATV212 (or ATV21) drive replacement

Product Line:
Altivar ATV21 and ATV212

Environment:
All

Cause:
Needs to replaced the basic control IO card that was in the ATV21 or ATV212 drive.

Resolution:
No. This part is not available to purchase in the US.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings