How can we help you today?

What is the difference between EZC250N and EZCV250N easy pact MCCB ?

The easy pact MCCB can be found into two types:

1- Normal easy pact supports protection against short circuit and overload currents.

2- Easy pact with built-in earth leakage protection in addition to the short circuit and overload currents.

EXC250N is Normal easy pact while the EZCV250N is a MCCB that supports earth leakage protection (built in).