How can we help you today?

What is the maximum breaking capacity for the ACB of type NW - 6300 A ?

The ACB of type NW with rating 6300 A has two breaking capacities:
1- 100 KA
2- 150 KA (Maximum breaking capacity)