Issue:
Preset Speeds on ATV61/ATV71 drives
Product Line:
ATV61 or ATV71
Environment:
All models, all serial numbers
Cause:
Application requires Preset Speeds
Resolution:
Refer to ATV61_programming_manual_EN_1760649_08
Preset Speeds on ATV61/ATV71 drives
Product Line:
ATV61 or ATV71
Environment:
All models, all serial numbers
Cause:
Application requires Preset Speeds
Resolution:
- Go into 1- Drive menu and then to 1.7 Application function menu.
- Under 1.7, go into Preset speeds submenu.
- Set 2,4,8, or 16 Preset speeds to logic inputs as desired.
Refer to ATV61_programming_manual_EN_1760649_08
Released for:Schneider Electric Nigeria