Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Econoflex FLEX58 drive be replaced?
Issue:
The FLEX58 drive used in the Econoflex has failed and needs to be replaced.

Product line:
Econoflex FLEX58

Environment:
All models, all serial numbers

Cause:
Attempting to maintain the Econoflex and change just the FLEX58 converter.

Resolution:
The FLEX58 is still a repairable product.  Recommend removing the FLEX58 from the Econoflex enclosure and sending it to our repair facility.
Another option is to replace the entire Econoflex with a comparable ATV660 or S-Flex (ATV212).

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings