Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the OC2P fault mean on the ATV21 and ATV212 Drives?

Issue:
ATV21/ATV212 OC2P fault

Product Line:
Altivar ATV21 and ATV212

Environment:
All

Cause:
Short circuit or grounding fault during deceleration

Resolution:
The fault means: Short circuit or grounding fault during deceleration
Drop the motor leads and Megger out the motor and cables with a 1KV Megger.
Run drive with no motor connected: Set 605 to 0 and measure voltage coming out of the drive at 20/40/60 hz intervals phase to phase voltage measurement.
Check for proper grounding at the motor and drive.