Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How can I get a run status on ATV212?

Issue:
Programming RY Relay for Run Status on ATV212 Drives.

Product line:
Altivar 212

Resolution:
Wire to RYA and RYC relay and program F130 to 14 (drive running).  The relay will close if a run command is issued and there are no faults.