Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the hole size of the padlock provision for a GV2P starter?
Issue:
Padlock hole diameter on GV2P

Product Line:
GV2 Manual Motor Protectors

Environment:
All GV2P, rotary handle.

Cause:
n/a

Resolution:
There are provisions for one padlock only, the hole size is approximately 6mm.  You can add a GV2V03 padlock attachment that will allow up to 6 padlocks for Lock out Tag out applications.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings