Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What causes an ILF code on an ATV61 or ATV71?
Issue:
Fault code ILF: Internal Link Fault

Product Line:
Altivar 61/71

Environment:
All models and serial numbers

Cause:
This fault appears when the communication between the option board and drive is interrupted

Resolution:
Internal serial link fault.
Check the +24v dc on control terminal board
Check the environment (electromagnetic compatibility).
Check the connections to make sure there are no shorts on terminal side.
Replace the installed option board.
Change the control terminal pod
Change the Main control board.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings