Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What causes an IFI fault on the ATV312 drive?

Issue:
Causes of an IFI fault on the ATV312 drive

Product Line:
Altivar, ATV312

Environment:
All

Cause:
Unknown rating

Resolution:
Try power cycling the drive to see if the IFI fault clears.  If it does not clear, replace the drive.
Reference manual BBV46385