How can we help you today?

Can we perform Automatic Transfer switch (1out of 2) using withdrawable version from MCCB of type NSX ?

- The ATS (Automatic transfer switch 1 out of 2) using the NSX MCCB can only be performed using:

1- Fixed MCCB NSX
2- plug in MCCB NSX

Attached here Catalog pages illustrate this info as well as connections for NSX ATS

Schneider Electric Nigeria

Attachment(s)
100 TO 630 NSX Source Changeover Assembly 00999531A 01.pdf [2.65 MB]
Source Changeover.pdf [361.89 KB]