How can we help you today?

What are the methods of Mechanical interlocks used with MCCB NSX ?

the methods of Mechanical interlocks used with MCCB NSX  can be one of the following:

1- Mechanical interlock on the frame of MCCB NSX for toggle operated breakers

2- Mechanical interlock on the frame of MCCB for rotary handle operated breakers

3- Mechanical interlock built in mounting plate for two fixed or plug in MCCB NSX (used for ATS 1 out of 2)