Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the S6X and Y suffix on the ATV61 drives?

Issue:
Needs to identify the difference between the S6X and Y suffix on the ATV61 drives

Product Line:
Alitvar ATV61

Environment:
All

Cause:
Input line voltage ratings

Resolution:
S6X suffix is 500 to 600VAC only
Y suffix is 575 to 690VAC only