Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find the RJ45 pin out for the ATV61/ATV71 drives?
Issue:
RJ45 pin out for ATV61/71 drives

Product Line:
All

Environment:
All

Cause:
Can not find documentation

Resolution:
The RJ45 connector uses two wire RS-485 connection for Modbus communications.
Pin 4 is the DB (+). Pin 5 is DA (-). These terminals are for communication.
Pin 7 is 10 VDC and 8 is 0 VDC. These are used to power the remote keypad when connected to this drive or the RS232 to RS485 adaptor when connecting from a PC with Powersuite.
The pins are numbered from Right to Left when looking at the front of the drive.

Schneider Electric Nigeria

Attachment(s)
Altivar 71 Intergrated Modbus 09080512142096779.pdf [657.85 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings