How can we help you today?

What is the marking principle of the components of the Sepam 1000+ range?

Issue

A user needs to understand how the identification markings on Sepam 1000+ software components and modules are structured and what information each part of the marking represents.

Product

  • Sepam 1000+
  • Sepam 1000+ Software Components
  • Sepam 1000+ Modules

Environment

  • Spare parts identification
  • Product ordering
  • Inventory management
  • Maintenance and service of Sepam 1000+ systems

Cause

Sepam 1000+ components are identified using a marking structure composed of multiple fields. Understanding these fields is necessary for ordering, stock management, product identification, and traceability.

Resolution

The components of the Sepam 1000+ range include both software and hardware modules. Each component is marked using five identification fields, with each field providing specific information about the component.

Example

59608 03146017FA DSM303 Remote Advanced UMI Module 0102003

The fields are interpreted as follows:

Reference Number: 59608 - Reference number used for purchase orders (P/O).

Stock Reference: 03146017FA - Internal stock reference number.

Commercial Reference: DSM303 - Commercial product designation.

Operational Reference: Remote Advanced UMI Module -Functional or operational description of the component.

Serial Number: 0102003 - Unique serial number used for identification and traceability.

By reading these five fields, users can accurately identify Sepam 1000+ components for procurement, maintenance, or replacement purposes.

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings