Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What file extensions are generated, and what do they mean, for each of the IEC61850 configuration files?

Issue
When creating the IEC61850 it creates different types of files.  What do they mean

Product Line
IEC61850
SEPAM
ION

Environment
Communication setup

Resolution
An IEC61850 configuration file will generate what is termed substation configuration language files, they are as follows:
1. ICD (Intelligent Capability description) or IED ( Intelligent Electronic Device) file
a. For each type of SEPAM device there is an ICD file. An ICD file describes all the functions and communication data available for the SEPAM.

2. CID (Configured IED Description) file
a. For every configured SEPAM or ECI850 device there is a CID file. It describes the operating IEC61850 configuration of the device.
b. A CID file is created when a device is configured with the configuration tool. The CID file is then loaded into the device to configure it. A CID file for an ECI850 contains configuration information for all the SEPAM devices to which it is connected.

3. SCD ( Substation Configuration Description)
a. An IEC61850 substation automation system has an SCD file. An SCD file contains configuration data for the IEC61850 system and the communication configuration settings for all related IEC61850 devices.


Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings