Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What do the colors within SFT2841 and the control matrix represent?


Product Line
SFT2841

Resolution
There are four colors that may be seen within SFT2841 in relation to options and selectivity, these colors also show a summary of the relay options within the control matrix:
White = Available to use
Red = Function/setting not enabled
Grey = Not selectable, typically due to pre-defined functionality
Black = Not available for that particular function/setting
Yellow = Not selectable, used by Logipam programming

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings