Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the ambient temperature requirements for power transformers to meet IEEE C57.12.00-2000?

According to the IEEE C57.12.00-2000 standard, power transformers are rated at a maximum ambient temperature of 40 degrees Celsius with the average ambient temperature not to exceed 30 degrees Celsius in any 24-hour period.