Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to use Easergy Configurator on a Windows 7 machine

In order to use the Easergy software within a Windows 7 environment, DosBox must be used. Run the installation for Easergy Configurator first, then using the instructions included in the DOSBOX file, install DosBox.
DOSBOX For Easergy.zipDOSBOX For Easergy.zipEasergy_Config_1_and_2.zipEasergy_Config_1_and_2.zip


Legacy KB System (APS) Data: RESL212992 V1.0, Originally authored by DaFr on 11/12/2013, Last Edited by DaFr on 11/12/2013
Related ranges: Others protection relays