How can we help you today?

How to move the 'ProWORX 32 Server' database files from one PC to another.

Issue
In the event that a customer wants to move the 'ProWORX 32 Server' from one PC to another PC, this
resolution will provide the list of files and folders that need to be moved after the ProWORX 32 Server
has been installed and authorized on the other PC..


Product Line
'ProWORX 32' Server


Environment
Windows 7, windows 10


Resolution
Copy the following folders from the ProWORX 32\Server folder on the source PC to the 'ProWORX 32\Server' folder on the destination PC.

Logs
Projects
Related Docs
User Profiles

Copy the following files from the ProWORX 32\Server folder on the source PC to the 'ProWORX 32\Server' folder on the destination PC.

UserDB.PWF
PlantLayout.PWF
prwxback.mdb
prwxbcresults.mdb
UserDB.p32
CSDatabase.p32
csdb.p32
FILELOCK.SYS
PlantLayout.ini
ServerActivityLog.txt

Copy the following files from the source PC to the target PC s
'ProWORX 32' folder.

Userdb.p32
Userdb.PWF