Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In Vijeo Designer, how many characters can I use for the project description?

Issue:
How many characters can be used for the project description in Vijeo Designer

Product Line:
Vijeo Designer


Resolution:
The project description field allow a maximum of 255 characters.