How can we help you today?

What is the baud rate switch settings for the Advantys STBNCO2212 CANopen NIM?

Issue:
How to set the baud rate on the Advantys STBNCO2212 CanOpen NIM.

Product line:
Advantys Configuration Software

Resolution:
When the lower switch is turned to any one of its baud rate positions, the baud rate is defined by the position on the upper switch. Only positions 0 through 7 are used to set the baud.
image

NOTE: The default baud in Flash memory for a new STBNCO2212 CANopen NIM is 1 Mbits/s.

Schneider Electric Nigeria