Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I make a backup of my XBTF Magelis application on my PCMCIA if I don't have the XBTL1000 software ?

Yes. Using Windows explorer simply insert the PCMCIA into a laptop. Copy the appli folder to a temporary folder. Now this appli folder can be copied onto any PCMCIA card and when inserted into the XBTF will load the saved application. Care must be taken when removing the PCMCIA from the laptop. The socket MUST be turned off before removing the PCMCIA card because it could sustain damage if removed hot.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings