How can we help you today?

Configuring the IP address of a TCSESM Connexium switch using the Command Line Interface.

Issue
Configuring the IP address of a TCSESM Connexium switch (i.e., TCSESM083F2CU0) using the Command
Line Interface.

Product Line
All ConneXium TCSESM switches

Environment
Windows 7, Windows 10

Resolution
The following procedure can be used to change the IP address of a ConneXium TCSESM switch
when the PC is connected to it using a V.24 cable.

  • Connect one end of the V.24 cable to the V.24 port on the switch and the other end to the PC's COM port..
  • Start 'Hyper Terminal' and open a connection using 9600, 8,None, 1 as shown below.
    qwf
  • Log into the switch using
Username: admin
Password: private
  • Type 'enable' at the prompt and hit the Enter key.
  • Type 'network protocol none' and hit the Enter key.
  • Type 'network parms <ip address> <network mask> <gateway address> and hit the Enter key.
  • Type 'copy system:running-config nvram:startup-config' and hit the Enter key.
  • Type ' y ' to answer the question on for saving the changes and hit the Enter key.
  • Type 'logout' and hit the Enter key.
  • Disconnect 'Hyper Terminal' from the switch.
err