Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What Modbus function codes are supported by the M340 line of PLCs?

The following Modbus function codes are supported by the M340 PLC line:
Function Code Description

1 Read output bits
2 Read input bits
3 Read output registers
4 Read input registers
15 Write output bits
16 Write registers