Issue
What is the value of Galvanic Insulation within TX-ports of Ethernet Connexium Switches (TCSESM)?
Product Line
Connexium TCSESM switches
Resolution
Vendor supplied specification is as follows:
Galvanic insulation is according to Ethernet standard IEEE802.3, 1500 VAC / 2250 VDC.
Released for: Schneider Electric Nigeria