Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I change the update rate of variables in the CoDeSys visualisation?

Goals and Symptoms

How can I change the update rate of variables in the CoDeSys visualisation?

Causes and Fixes

CoDeSys:
For using the CoDeSys-visualisation, the CoDeSys.ini file has to be changed. The entry "UpdateRage" has to be insert/changed:
[CoDeSys]
UpdateRate=200

CoDeSysHMI:
For CoDeSys HMI, the entry has to be done in CoDeSysHMI.ini:
[CoDeSysHMI]
UpdateRate=200

WebVisu:
In case of the Web-Visu, the value has to be changed in WebVisu.htm:
<param name="UPDATETIME" value="200">

The default value for each visualisation is 200 ms.