Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is PL7 software supported under Microsoft Windows 7 operating system?

Issue:
PL7 software supported under Microsoft Windows 7 operating system


Product Line:
PL7 software


Resolution:
Yes, PL7 is supported under Window 7 32 bit operating system with the install of SP5 of PL7. Windows 7 64 bit is not supported

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings