How can we help you today?

Isolation specifications for the ETG100.

Issue
Isolation specifications for the ETG100.

Product Line
TSXETG100

Environment
Windows 7


Resolution
The following are the isolation specifications for the ETG100.

  • Isolation between the Ethernet POE input and +24Vdc input is 1500V.
  • Isolation between the power inputs (POE and +24) and the isolated comms supply is 2500V.
  • Isolation between the Ethernet input and the serial port is 1500V.
  • There is only one serial port on the TSXETG100 with 2 hardware interfaces, isolation between the interfaces is 2500Vrms

Schneider Electric Nigeria