Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In Vijeo Designer, how can I retain the link to a Linked Variable file?


Issue:
How to retain the link to a Linked Variable file in Vijeo Designer

Product Line:
Vijeo Designer

Resolution:
Any time you export a project to a VDZ file, you will lose the Link Variable file. To retain the link, you need to copy the SWXCF file from the original
project folder and copy the file to project folder in the destination machine. Also make sure that the drive letter used in the link is also available on
the destination machine otherwise you will need to map the drive.