Product:
M340
Answer:
The proprietary TCP port number for Modbus/TCP traffic for the M340 BMXP342020 processor's native ethernet port is 502.
Released for: Schneider Electric Nigeria


Our Brands
Welcome to the Schneider Electric Website
Product:
M340
Answer:
The proprietary TCP port number for Modbus/TCP traffic for the M340 BMXP342020 processor's native ethernet port is 502.
Discuss this topic with experts