Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
It appears that communications is intermittent and the unit is not responding appropriately.

Possible problem and solution:

The VW3L3P01R40 cable has a five-volt DC input, which should be used if intermittent or no communication is encountered.
Use a 5 VDC regulated power supply with at least 50 mA current.
The power jack is for a 2.5 mm diameter plug center polarized connector.

Be sure to check the baud rate set in Lexum CT, and be sure it is the same as the Lexium ILP/ILT baud rate setting.


Legacy KB System (APS) Data: RESL200114 V1.0, Originally authored by MaPr on 09/28/2009, Last Edited by MaPr on 09/28/2009
Related ranges: Lexium ILT, ILP