Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the meaning of the following error numbers ? B300, B301, B302, B303, B304, B305, B306, B307, B308, B309, B30A, B30B, B30C, B30D, B30E, B30...

Goals and Symptoms

What is the meaning of the following error numbers ?

B300, B301, B302, B303, B304, B305, B306, B307, B308, B309, B30A, B30B, B30C, B30D, B30E, B30F, B310

Causes and Fixes

A Detailed description is available in the attched power point presentation.

Attachments

(Removed File URL: 202829_F202/LXM05B-B3xx_error_numbers.ppt)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/3616d1092a0322a8c1257754003ca70a/fl_block_5/0.634?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL202829 V1.0, Originally authored by StKu on 07/02/2010, Last Edited by StKu on 07/02/2010
Related ranges: Lexium 05

Schneider Electric Nigeria

Attachment(s)
LXM05B-B3xx_error_numbers.ppt [111 KB]