Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to calculate the minimum and maximum slave position when using AFB FlyingShear ?

Goals and Symptoms

How to calculate the minimum and maximum slave position when using AFB FlyingShear ?

Causes and Fixes

There is a program example available which contains a function block for calculating this two values. See attachment or M&D TIP database "Programming Examples".

Schneider Electric Nigeria

Attachment(s)
2010-07-14_GetMinMaxSlavePos_FS.zip [1.36 MB]
FlyingShear_GetMinMaxSlavePosition.ppt [83 KB]