Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Goal: pin diagram of ATS48 RJ 45 connector. I would like to have the pin diagram of ATS48 RJ 45 connector RS 485 cable. I will be happy if you can se...

Goals and Symptoms

Goal: pin diagram of ATS48 RJ 45 connector. I would like to have the pin diagram of ATS48 RJ 45 connector RS 485 cable. I will be happy if you can send. Best regards, Asli

Facts and Changes

pin diagram of ATS48

Causes and Fixes

Since ATV28, the RJ45 is a standard for all PRODUCTS ( VVD and PCP ) so:

1 -
2 -
3 -
4 - D(B)
5 - D(A)
6 -
7 - 10v
8 - 0v


Legacy KB System (APS) Data: RESL156927 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48