Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many is the max value (peak) intensity of current on a ATV38C10N4 when I supply the ATV WITHOUT Motor connected?

Goals and Symptoms

How many is the max value (peak) intensity of current on a ATV38C10N4 when I supply the ATV WITHOUT Motor connected?

Facts and Changes

ATV38C10N4
courant peak max

Causes and Fixes

la valeur peak du courant de ligne à la mise sous tension du produit sans moteur est environs = 340A .
voir les relevés en fichier attaché:

Attachments

(Removed File URL: 159699_40EA/ATV38_courant_de_demarrage.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/e56cc7d792ddaf4985256e40004f43e5/fl_block_5/0.13D2?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL159699 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 38

Schneider Electric Nigeria

Attachment(s)
ATV38_courant_de_demarrage.zip [11.41 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings