Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum current draw (amps) at CL1 and CL2 at 115VAC for each ATS48 model?

Goals and Symptoms

What is the maximum current draw (amps) at CL1 and CL2 at 115VAC for each ATS48 model?

Facts and Changes

ATS48 CL1 and CL2 power with cooling fans working

Causes and Fixes

For each card without fan under 115 Vac: 220 mA

With fans:

D32 to C17 : 260 mA
C21 to C32 : 440 mA
C41 to M12 : 700 mA


Legacy KB System (APS) Data: RESL160577 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48