Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Speed drive - Speed range ATV

Goals and Symptoms

Speed drive - Speed range
ATV

Causes and Fixes

For a speed drive, the speed range is the ratio between the output maximum frequency and the minimum frequency where the nominal torque is available.

example for a 50Hz motor :

Speed range 1/50 means the drive is able to give the nominal torque between 1Hz to 50Hz.

Speed range 1/100 means the drive is able to give the nominal torque between 0.5Hz to 50Hz.


Legacy KB System (APS) Data: RESL160729 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58