Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ProWorx 884 software have a compare utility?

Issue

Does the ProWorx 884 software have a compare utility?

Product Line

ProWorx

Environment

ProWorx 884

Resolution

Yes. The ProWorx 884 software has a network file compare utility that can compare the networks from file 1 with those from file 2. This is a three pass comparison that tests for unchanged networks, moved networks and networks that have been edited. This option also builds a table of network numbers comparing file 1 to file 2. From this table the mismatched networks may be displayed or printed.