Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What replaces the AS-BADU-212?

Issue

What replaces the AS-BADU-212?

Product Line

Compact

Environment

AS-BADU-212

Resolution

Component obsolescence has necessitated the AS-BADU-212 be removed from active sales. For new applications other analog input modules from the Compact line may be utilized:
For 4-20 mA and +/- 10V applications, either the AS-BADU-206 or AS-BADU-256 may be used as a replacement. (The AS-BADU-256 functions just like the AS-BADU-206 except the AS-BADU-256 operates at extended temperature).
For thermocouple and RTD applications, the AS-BADU-257 may be used as a replacement.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings