Issue
What is the operating temperature range for the Quantum I/O modules?
Product Line
Modicon Quantum
Environment
Quantum
Resolution
The operating temperature range for the Quantum I/O modules is.....0 to 60° C (32 to 140° F).
Released for: Schneider Electric Nigeria