Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
FTX ES 00 Software Restrictions

Issue

The purpose of this resolution is to inform Advantys STB users of restrictions regarding FTX ES 00 software.

Product Line

The FTX ES 00 is free software that does not require registration. It contains the OTB/FTM software and
the STB Lite version configuration software.

STB Lite software is a demonstration version. If using it, you cannot go online, nor download. It cannot be
converted to a full version by merely transferring registration. You need to install the full version before attempting
an authorization transfer.

Resolution

Reference the attached document for information on how FTX ES 00 and STBSPU1000 can coexist in the same PC.

STB & FTX.doc


Legacy KB System (APS) Data: RESL170483 V3.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB