Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What programming software is required to support the TSX07 Nano PLC?

Article available in these languages: Japanese

Issue
Need to identify the programming software for the TSX07 Nano PLC.

Product line
PL7-07, TSX Nano

Environment
TLXLPL707P40M

Resolution
PL7-07 is required to support the TSX 07 Nano PLC. The part number for a single install is TLXLPL707P40M. Note that this is an obsolete DOS based software. There is no windows based equivalent software.