Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there any way to display used references in a Modsoft program while OFF-LINE from the controller?

Issue
Is there any way to display used references in a Modsoft program while OFF-LINE from the controller?

Product line
Modsoft

Environment
Modsoft

Resolution
No. Modsoft can display used references in a PLC program only while ON-LINE with a controller. Modsoft can also print out used references as part of printing a program, but cannot dispaly them while OFF-LINE from a controller. To display the Used References while on-line with a controller, first go open any ladder logic network ,then select "Refs" from the top tool-bar. The "Used References" option will appear in that pull-down menu.