Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the Telefast fuse part numbers?

The following fuse part numbers are used in the Telefast 2 PreWired System Connection Interfaces:

Fuse Rating
Part Number
0.125 A
ABE7FU012
0.5 A
ABE7FU050
1 A
ABE7FU100
2 A
ABE7FU200
4 A
ABE7FU400
6.3 A
ABE7FU630

These fuses are fast blow, 5 x 20mm, 250V and have a quantity of 10 per package.